eo_logo
  • Country/Region
  • cart   
 
Edmund Optics® manufactures optical components used in antibody detection. Inquiries about complete systems should be directed to the antibody detection device manufacturers.

Case Study:
Optics for Antibody Detection

The future depends on quick and accurate detection of antibodies to determine if subjects have had an immune response to contagious diseases, such as COVID-19 (novel coronavirus).

Identifying Immune
Response to COVID-19

Serological (blood-derived) testing can look for antibodies specific to COVID-19, the disease caused by the novel coronavirus.

Antibodies are Y-shaped proteins produced by white blood cells to help stop a virus from intruding. The human body produces different types of antibodies, some of which are temporary, but others remember how they responded to an infection and can attack again if exposed to the same pathogen.1

Immunoglobulin M (IgM) is one of the first antibodies that the body makes when fighting a virus, but it fades out as the infection goes away. The immunoglobulin G (IgG) antibody is produced second and can be found in the blood of people who are tested after infection, showing that they have had an immune response to the infection.2 This is especially important for detecting infections for which a person showed few or no symptoms.3 While it is not known if the presence of antibodies will provide immunity from a future infection, serological tests are crucial for determining the extent of the spread of COVID-19 and providing data required to properly respond and combat this pandemic.  

Quick, Reliable, and Accurate COVID-19 Testing
Figure 1: Y-shaped antibodies attacking a virus.

How Do Antibody Detection Tests Work?

Two common serological diagnostic methods for novel coronavirus are an enzyme-linked immunosorbent assay (ELISA) and an indirect fluorescent antibody test (IFA).

The direct ELISA method requires a patient’s blood to be drawn and then typically sent to a lab where it is processed into a serum.4 A well plate is then prepared with an immobilized synthetic spike protein with a similar shape to novel coronavirus. The serum is then added to the well plate and the IgM and IgG antibodies bind with the antigen. Unbound antibodies are washed away. A chemical liquid is also added which changes color if antibodies have bound to the target antigen. The color changes at a rate proportional to the amount of antigen-specific antibody in the specimen. Color intensity can be assessed visually or spectrophotometrically with an immunoassay reader (pictured at the top of Figure 2).

SpectralMD’s wound imaging system in use
Figure 2: Direct ELISA process in which color change indicates the presence of antibodies.

The second, and more advantageous serological diagnostic method, is the indirect fluorescent antibody test (IFA).

The steps of the IFA are very similar to those of the ELISA. Both virus-infected and uninfected cells are fixed to wells in a glass slide. As with the ELISA method, unbound antibodies are removed by washing. The binding of primary antibodies to the slide wells in the IFA method is demonstrated by using a fluorescent dye-conjugated anti-immunoglobulin. After washing away any unbound conjugate, slides are covered with buffered glycerol and examined with a fluorescence microscope. The morphology and location of fluorescence can be evaluated to differentiate specific reactions from nonspecific reactions (Figure 3). This is not true for most other serological tests and is a major advantage of the IFA method.5

SpectralMD’s wound imaging system in use
Figure 3: Indirect immunofluorescence test of antibodies.

Many immunoassay readers for the ELISA and IFA methods rely on fluorescence or color changes from enzyme reactions and follow a similar schematic to fluorescence microscopes (Figure 4). Examples of prominent companies that support immunofluorescence applications include BioTek Instruments, Molecular Devices, Essen BioScience, and Thermo Fisher Scientific.

The optical designs of fluorescence-based or color detection screening systems for ELISA and IFA methods resemble this setup of a simple fluorescence microscope.
Figure 4: The optical designs of fluorescence-based or color detection screening systems for ELISA and IFA methods resemble this setup of a simple fluorescence microscope.

An excitation filter allows the passage of wavelengths from an illumination source that would excite the fluorescent sample. These excitation wavelengths reflect off of a dichroic filter and are focused onto the sample by lenses. Fluorescent emission from the sample transmits through the dichroic filter towards lenses that focus the light onto the system’s detectors. Measuring the amount of fluorescence lets the immunoassay reader determine the presence of COVID-19 antibodies that would indicate if a patient had the virus.  

Edmund Optics proudly supplies optical components for COVID-19 diagnostics. These devices, along with countless other optics-enabled technologies, are helping create a safer and healthier future.

References

1. Healthwise. (2019, December 8). Immunoglobulins. Retrieved from University of Michigan, Michigan Medicine: https://www.uofmhealth.org/health-library/hw41342

2. FDA. (2020, May 13). FAQs on Testing for SARS-CoV-2. Retrieved from FDA Medical Devices: https://www.fda.gov/medical-devices/emergency-situations-medical-devices/faqs-testing-sars-cov-2#serology

3. CDC. (2020, May 5). Serology Testing for COVID-19. Retrieved from Centers for Disease Control and Prevention: https://www.cdc.gov/coronavirus/2019-ncov/lab/serology-testing.html

4. Udugama, K. K. (2020). Diagnosing COVID-19: The Disease and Tools for Detection. ACS Nano, 14. Retrieved from https://pubs.acs.org/doi/10.1021/acsnano.0c02624

5. Charles River Laboratories International. (2016). Serologic Methods Manual. Retrieved from Charles River Laboratories International: https://www.criver.com/sites/default/files/resources/SerologicMethodsManual.pdf

Was this content useful to you?
The Future depends on optics

Need a Quote? Add a stock number to begin our two-step quote process.

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram Edmund Optics Tick Tock



SELECTION OF OUR MEMBERSHIPS:

Spectaris Optence Photonics21 Epic EMVA EOS Photonics FranceCLP

×