Edmund Optics uses cookies to optimise and enhance the features and content on our website. By continuing to use this website, you consent to our use of cookies.

  • My Account
  •   
Company / Press Releases / Press Releases / II-VI and Edmund Optics Collaborating to Make IR Optics More Accessible than Ever Before

II-VI and Edmund Optics Collaborating to Make IR Optics More Accessible than Ever Before

IR Optics Available Immediately
2/12/2019, Mainz, Germany   —

Edmund Optics® (EO), the premier provider of optical components, announces a collaboration with II-VI Incorporated to provide immediate delivery of Zinc Selenide (ZnSe) optical components. Zinc Selenide (ZnSe) Plano-Convex (PCX) Lenses, Zinc Selenide (ZnSe) Aspheric Lenses, CO2 Beam Expanders, and Lens Stress Analyzers are now available.

This collaboration makes it easier than ever before to purchase optical components for infrared applications throughout the design, prototyping, and production project cycles.

TECHSPEC® Zinc Selenide (ZnSe) Plano-Convex (PCX) Lenses are designed by EO and manufactured by II-VI out of premier grade ZnSe material with <0,0005 cm-1 bulk absorption at 10,6 µm. They are available uncoated or coated with broadband anti-reflection coatings for 8-12 µm or 3-12 µm. Their irregularity of <λ/20 at 10,6 µm and surface roughness of <50Å makes them ideal for precision IR applications.

Similarly, the TECHSPEC® Zinc Selenide (ZnSe) Aspheric Lenses are also designed by EO and manufactured out of the same premier grade ZnSe. While offering the same surface specifications and 8-12 µm AR coating option as the ZnSe PCX Lenses, the TECHSPEC® Zinc Selenide (ZnSe) Aspheric Lenses feature diffraction-limited performance for minimum focused spot sizes.

The CO2 Beam Expanders are constructed out of more premier grade ZnSe optical elements for collimating and improving the energy distribution of high power CO2 laser beams at 10,6 µm. The beam expanders feature minimized beam deviation and AR coatings that result in 99,4 % transmission and <0,1% absorbance per surface at 10,6 μm.

The final new II-VI product offered by EO are Lens Stress Analyzers, which utilize cross polarization to identify mechanical stress, thermal stress, and contamination. They are available in either a portable, clip-on design or a bench-top model, ideal for lab settings.

Information about Edmund Optics:

Edmund Optics® is a leading global manufacturer and distributor of precision optics, optical assemblies and image processing components with headquarters in the USA and manufacturing facilities in the U.S., Asia and Europe and sales representatives around the globe. EO has the world's largest inventory of optical components for immediate delivery and offers products, standard or customized, in small quantities but also in volume for various industries. Request a quote or place your order through the website www.edmundoptics.eu or contact us via phone +49 (0)6131 5700 0 or email [email protected] by reference to our catalogue.

EO adds thousands of new products each year! Look for our newest arrivals marked with the New Products icon!

Since 1942, EO has been a leading supplier of optics and optical components. Learn more about our past, present, and future!

Need a Quote?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram



×