eo_logo
  • Country/Region
  • cart   
 
BRAIN
 

BRAIN

Optics and Brain Diagnostics Advancements

The brain is the most powerful organ in the human body. It is the center of our nervous system and controls all of our voluntary and involuntary bodily functions. The brain controls all other organ functions, generates muscle activity, and controls the secretion of hormones. From simple reflexes to complex sensory input, the brain and its billions of neurons are always in control. Due to advances in optics and medical diagnostics, how each neuron and glial cell interact is now better understood than ever, but how millions of neural networks operate as a single unit for complex tasks remains a mystery for researchers. More tools than ever before are available to image brain slices and utilize less invasive fiber-coupled imaging systems to understand how the brain works electrically, chemically, and physically. The key components to imaging brain slices and fiber-coupled imaging systems are infinity corrected, apochromatic microscope objectives with high magnifications and high numerical apertures.

View Products

Blood and Optics

Ailments of the Brain

Below are common ailments of the brain that are detected by advanced diagnostic techniques such as fluorescence microscopy. Advancements in microscope objectives and other optical components allow these ailments to be more easily detected and treated.

Stroke

Medical condition caused when blood supply to the brain is interrupted for an extended period of time, resulting in muscle weakness on one side of the body, loss of face control, numbness, and speech issues.

Alzheimer’s

Progressive and incurable type of dementia that destroys memory and other important mental functions, beginning slowly and worsening over time.

Parkinson’s

Incurable disorder of the central nervous system (CNS) that affects movement and includes uncontrollable tremors.

Huntington’s

Inherited, incurable condition that causes nerve cells in the brain to break down over time, causing jerky body movements and eventually the inability to talk.

Meningitis

Severe inflammation of the brain and spinal cord membranes that is typically onset by an infection and leads to fever, headache, and neck stiffness.

Epilepsy

Condition characterized by recurring seizures mainly due to abnormal and increased electrical activity in the brain.

Concussion

The most common type of traumatic brain injury, onset by heavy impact resulting in the brain shaking or moving inside the skull.

Brain Tumors

Cancerous or non-cancerous growths of abnormal cells in the brain with a variety of severity levels and types including astrocytoma, blastoma, ependymoma, and meningioma.

Diagnostic Techniques

Many diagnostic techniques are used to examine, diagnose, and treat the brain including laser-based microscopy, optogenetics, and CLARITY.

GFP

Green fluorescent protein (GFP) is a specialized protein consisting of a specific group of amino acids that glows green when exposed to UV or blue light. Extracted from marine life, the most common excitation wavelength is 395nm to 475nm with emission peaks from 509nm to 525nm. GFP is widely used in non-invasive fluorescence imaging systems to detect tumor growth, apoptosis, and other cellular activity.

Optogenetics

Biological technique that involves the use of light to control cells in living tissue, specifically neurons, in most cases that have been genetically modified with photoreceptors that react to different wavebands.

CLARITY

Method of making brain tissue transparent using hydrogels. Accompanied with antibodies or biomarkers, highly detailed pictures of nucleic structure of the brain can be determined and studied.

GCaMP

A genetically encoded calcium indicator used in brain imaging. GCaMP is similar to the fusion of green fluorescent protein (GFP), calmodulin, and a peptide sequence from myosin.

Brain Mapping

Neuroscience technique intended to map and list out the specific quantities or properties of the brain in a spatial representation. In other terms, the anatomy and function of the brain, spine, and central nervous system through imaging techniques.

Patch Clamp

Electrophysiology technique allowing the study of single and multiple ion channels in neurons, cardiomyocytes, muscle fibers, and other cells.

Laser-Based Microscopy

Microscopy techniques such as fluorescence, confocal, multiphoton, and super resolution microscopy are used for the study of synapses, neurons, and neural circuits in brain slices.

Diagnostic Techniques

Example Technique: Fluorescence Confocal Microscopy

Fluorescence microscopy is one of the primary techniques used to study the functional or morphological dynamics of synaptic structures, including dendritic spines and axon terminals, and to characterize circuit connectivity and dynamics. Typically, a laser beam is focused into a pinhole, acting as a point source illuminator. Spatially filtered light is reflected by a dichroic filter, which may or may not require a beam expander to fill the entire aperture of the objective. The objective then focuses excitation energy onto the sample, which emits a weaker fluorescence signal collected by the same objective. This emission light is transmitted through the dichroic filter into the secondary tube lens and then passes through a final pinhole before detection by a CCD or CMOS sensor. Ideally, both pinholes are located in conjugate image plans on the optical axis, which allows the images to overlap perfectly on the object plane. Since confocal microscopes observe a very thin, small spot in the object plane, it is important to sample light via a scanning system or motorized actuator to collect an array of images. These images are then reconstructed into 2D or 3D images.

Flow Cytometry
Figure 1: Basic Optical Filtering Arrangement for Fluorescence Microscopy

Fluorescence Microscopy: In-Line Illumination with Imaging Filters

Learn more about how to assemble a fluorescence microscopy system.

Infinite Conjugate Tube Length Calculator

Determine the maximum tube length in an infinite conjugate microscope system for covering a specific image sensor size without vignetting using the objective focal length, objective NA, tube lens entrance pupil diameter, tube lens focal length, and sensor size.

Product Spotlight

Multi-element objectives are critical for any microscopy technique, including many diagnostic techniques for the brain. Understanding the different types of objectives is important in order to ensure you are using the correct objective for your application.

Finite Conjugate Objectives

Finite Conjugate Objectives

Finite Conjugate Objectives are microscope objectives that do not require a secondary lens to focus onto a specimen. They are typically optimized for use in the visible spectrum and contain up to four lens elements.

Figure 2: Finite Conjugate Microscope Design

View Product

Technical Article Icon

Understanding Microscopes and Objectives

READ
Infinity Corrected Objectives

Infinity Corrected Objectives

Infinity Corrected Objectives are microscope objectives that focus at infinity. They offer long working distances, along with the ability to place optical components, such as optical lenses or optical filters, into the optical path. Infinity Corrected Objectives feature higher resolutions than Finite Conjugate Objectives, but are heavier and more expensive.

Figure 3 (left): Infinite Conjugate (Infinity Corrected) Microscope Design

View Product

Technical Article Icon

Understanding Microscopes and Objectives

READ
Technical Article Icon

Understanding Infinity Corrected Objective Resolving Power and Magnification

READ
Technical Article Icon

Using Tube Lenses with Infinity Corrected Objectives

READ
Reflective Objectives

Reflective Objectives

Reflective Objectives are microscope objectives that use two mirrors to form an image or focus a laser in microscopy applications requiring chromatic correction over broad spectral ranges.

Figure 4: Anatomy of a Reflective Objective

View Product

Technical Article Icon

Understanding Microscopes and Objectives

READ
Technical Article Icon

Introduction to Reflective Objectives

READ
Technical Article Icon

Demanding Applications Call for Reflective Objectives

READ
Achromatic Objectives

Achromatic Objectives

Achromatic Objectives are microscope objectives that correct for chromatic aberration in red and blue wavelengths, and spherical aberration in the green wavelength. Achromatic Objectives are lighter and cheaper than Apochromatic Objectives, but do not have as much correction for chromatic aberration, spherical aberration, and field flatness.

Figure 5: Apochromatic (Left) vs. Achromatic (Right) Objective Designs

View Product

Technical Article Icon

Understanding Microscopes and Objectives

READ
Apochromatic Objectives

Apochromatic Objectives

Apochromatic Objectives are microscope objectives that feature better color correction than Achromatic Objectives over a broad wavelength range (VIS to NIR), along with better spherical correction and field flatness. However, they are heavier and more expensive than Achromatic Objectives.

Figure 6: Apochromatic (Left) vs. Achromatic (Right) Objective Design

View Product

Technical Article Icon

Understanding Microscopes and Objectives

READ

Edmund Optics® Mission for Brain Diagnostics

  • Design and manufacture optics to improve global brain health
  • Facilitate optical system development to correctly diagnose neglected and emerging brain diseases around the world such as strokes, Alzheimer’s, Parkinson’s, Huntington’s, Meningitis, Epilepsy, and brain tumors
  • Enable easy-to-use optical devices for physicians, neurologists, nurses, or technicians to quickly and accurately diagnose with the push of a button
  • Research and develop innovative optical components to advance point of care devices for impoverished regions or populations without access to modern healthcare
  • Advance noninvasive optical diagnostics techniques to reduce the global burden that brain diseases cause on general health

Need a Quote? Add a stock number to begin our two-step quote process.

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram Edmund Optics Tick Tock



SELECTION OF OUR MEMBERSHIPS:

Spectaris Optence Photonics21 Epic EMVA EOS Photonics FranceCLP

×