Edmund Optics uses cookies to optimise and enhance the features and content on our website. By continuing to use this website, you consent to our use of cookies.

  • My Account
  •   
Resource Page / Application Notes / Microscopy / Using Tube Lenses with Infinity Corrected Objectives
Using Tube Lenses with Infinity Corrected Objectives
Edmund Optics Inc.

Using Tube Lenses with Infinity Corrected Objectives

Using Tube Lenses with Infinity Corrected Objectives

In order to create an image with an infinity corrected objective, a tube lens must be used to focus the image. One advantage to using an infinity corrected objective with a tube lens is that there can be a space between the objective and tube lens. The space allows additional optical components to be inserted into the system, such as optical filters or beamsplitters. The distance between the objective and the tube lens (L) can be varied, but this will affect the image field diameter (∅). Equations 1 and 2 are approximation formulas to determine the relation between ∅ and L.

(1)$$ ∅_1 \left[ \text{mm} \right] = 2 F_1 \cdot \text{NA} $$
(2)$$ L \left[ \text{mm} \right] = \frac{\left(∅_2 - ∅_1 \right) F_2}{∅} $$

 

Where,
1 (mm) is the exit pupil diameter of the objective
2 (mm) is the entrance pupil of the tube lens
F1 (mm) is the focal length of the objective
F2 (mm) is the focal length of the tube lens
NA is the Numerical Aperture of the objective

Application Example

Question: Using an M Plan APO 10X objective (#46-144), MT-1 tube lens (#54-774), and a 2/3” sensor camera, what is the maximum spacing between the tube lens and objective without vignetting?

Answer: The focal length of the objective (F1) is 20mm and NA is 0.28, so the exit pupil diameter can be calculated:

(3)$$ ∅_1 = 2 \cdot 20 \text{mm} \cdot 0.28 = 11.2 \text{mm} $$

 

A 2/3” image sensor features an 11mm diagonal, therefore ∅ needs to be at least 11mm. The focal length of the MT-1 tube lens is 200mm and the entrance pupil diameter is 24mm. Therefore,

(4)$$ L = \frac{ \left( 24 \text{mm} - 11.2 \text{mm} \right) 200 \text{mm} }{11 \text{mm}} = 232.7 \text{mm}$$

 

As long as the spacing between the tube lens and objective is less than 232.7mm, there will be no vignetting.

Was this content useful to you?

Think microscopes are only used for introductory biology lessons? Learn about them and their diverse uses in the optics, imaging, and photonics industries.

Get training tips on using different illumination techniques to help with all your microscopy applications. (PDF 898KB)

Long working distance microscopy objectives for the UV, visible, or IR spectrum from manufacturers such as Mitutoyo, Olympus, or Nikon.

From biometrics to DNA sequencing to in-vitro diagnostics, quality products, technical content, and expertise from a single bio source.

Need to contact Edmund Optics? Use any of our fast and friendly services to meet your needs.

Need a Quote?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram



×