Edmund Optics uses cookies to optimise and enhance the features and content on our website. By continuing to use this website, you consent to our use of cookies.

  • My Account
  •   
Resource Page / Glossary / U

Glossary: U

Ultraviolet (UV) Spectrum

The wavelength interval of the electromagnetic spectrum that corresponds to ultraviolet light (light that is beyond the visible violet range). UV radiation is often divided into three smaller regions: 320 - 400nm, 280 - 320nm, and 100 - 280nm – defined as UV-A, UV-B, and UV-C, respectively.

Unpolarized

Characterization of light that contains random combinations of x and y components of the electric field. Light from sources such as incandescent and fluorescent bulbs, LED spotlights, fiber optic illuminators and sunlight are all examples of unpolarized light.

  See also Polarization

Spherical optics, aspheric lenses, prisms, imaging lenses, imaging and laser optics assemblies, and mechanics are just a few of our expertise.

Edmund Optics' engineers are experts in delivering the best solution possible. From stock products to custom designs, EO has the industry and technical knowledge to help meet your needs.

Over 15 regional offices in the Americas, Europe, and Asia to offer local support with world-class service.

Need to contact Edmund Optics? Use any of our fast and friendly services to meet your needs.

Need a Quote?

Edmund Optics Facebook Edmund Optics Twitter Edmund Optics YouTube Edmund Optics LinkedIn Edmund Optics Instagram



×