Edmund Optics®, a leading global supplier of optical components and solutions, has expanded and diversified its extensive product inventory by introducing a range of Digital Fiber Coupled LEDs. This addition broadens the options available in fiber-coupled lighting solutions, bridging the gap between affordability and high functionality.
Offering a compact, high radiant power solution for applications including spectroscopy, optogenetics, and fluorescence, the Digital Fiber Coupled LEDs provide significant advantages over the conventional analog solutions typically employed by researchers and engineers.
Their built-in software is compatible with LabVIEW, MATLAB, and Python, making integration into existing lab setups straightforward. With passive thermal management, the LEDs operate without fans or replacement lamps, reducing noise and the need for frequent maintenance compared to traditional setups.
The all-in-one design simplifies installation and use, streamlining workflows for researchers and engineers. "We added these Digital Fiber Coupled LEDs to provide a practical, easy-to-use, and cost-effective option that requires minimal setup and offers high precision," said Gregg Fales, Director, Marketplace Product at Edmund Optics.
Covering wavelengths from 275 to 940 nm, these Digital Fiber Coupled LEDs deliver up to 250 mW of output power and include an integrated driver and controller. They provide full control over output power, pulse duration, and other settings without the need for extra hardware.
With this launch, Edmund Optics reinforces its commitment to delivering innovative and accessible optical solutions, empowering researchers and engineers with high-precision tools that are both affordable and easy to integrate.
To view these, and many more exciting new products from Edmund Optics, visit the new products page at www.edmundoptics.com.
About Edmund Optics:
Edmund Optics® is a leading global supplier of optics, imaging, and photonics technology that has served a variety of markets including Life Sciences, Biomedical, Industrial Inspection, Semiconductor, R&D, and Defense since 1942. The company designs and manufactures a wide array of optical components, multi-element lenses, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of stock and custom products. Operating in more than a dozen major facilities around the globe, Edmund Optics employs just over 1,100 employees and continues to expand. Customers can purchase items by calling 1-800-363-1992, via the catalog, or on the website at www.edmundoptics.com.